Sök bland vanliga frågor (FAQ)
Is ATV630xxxN4EU supported by ATV600 DTM in SoMove?
Issue:
DTM file used for the ATV630xxxN4EU in SoMove.
Product Line:
AVT600, ATV630
Environment:
All
Cause:
NA
Resolution:
ATV630xxxN4EU drives are not supported by ATV600 DTM.
If customer wants a drive supported by SoMove, then it needs to be replaced with an ATV650xxxN4EU.
DTM file used for the ATV630xxxN4EU in SoMove.
Product Line:
AVT600, ATV630
Environment:
All
Cause:
NA
Resolution:
ATV630xxxN4EU drives are not supported by ATV600 DTM.
If customer wants a drive supported by SoMove, then it needs to be replaced with an ATV650xxxN4EU.
Publicerad för:Schneider Electric Sverige
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj