How to setup an Alarm Variable in EcoStruxure Operator Terminal Expert (formerly known as Vijeo XD)?
Issue:
Cannot find where in EcoStruxure Operator Terminal Expert (formerly known as Vijeo XD) to create an Alarm Variable.

Product Line:
EcoStruxure Operator Terminal Expert, Vijeo XD 3.0 or higher.

Resolution:




In order to setup an Alarm Variable in Vijeo XD, there are a few steps you need to make.

1) First create an Alarm Group by first selecting "Alarms / Events" and then press the + Alarm Group button

2) Create a variable to use as the Alarm Variable
3) Expand the Alarm Group and choose the type of alarm you would like to create (BOOL / LEVEL)
4) Press the +Alarm Button to add the variable that you created. (See below)

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj