What can cause an CFI3 or Pre-setting transfer error on the ATV630 and ATV930 Process Drives?

Article available in these languages: Spanska

Issue:
CFI3 or Pre-setting transfer error causes on the ATV630 and ATV930 Process Drives.

Product Line:
ATV630 and ATV930 Process Drives

Environment:
All

Cause:
• The configuration transfer to the drive was not successful or interrupted.
• The stored pre-set was loaded from an different firmware (MCP/MCE), with additional, less parameters.

Resolution:
Principle
The pre-setting transfer error occurs if a pre-set file could not be loaded to the device, or the configuration is not compatible.
Probable cause
• The configuration transfer to the drive was not successful or interrupted.
• The stored pre-set was loaded from an different firmware (MCP/MCE), with additional or less parameters.

Remedy
• Load a compatible configuration.
• Check the pre set file
• Use SoMove to transfer pre-set to the device
• perform a factory setting

Schneider Electric Sverige

Utforska mer
Kategori:
Artiklar som kan vara till nytta
Utforska mer
Kategori: