Sök bland vanliga frågor (FAQ)
How to import the Ecodial design file (.ELV) file in Ecoreach?
One of the following ways can be used to import the .ELV file
1) Drag and drop the .ELV file
2) Click browse to import the .ELV file
If the import is successful, the devices in the .ELV file appears in the discovered devices section.
If the import is unsuccessful, ‘Unable to import the selected file’ error message is displayed.
Publicerad för:Schneider Electric Sverige
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj