What is the difference between Pixel Resolution and Display Resolution?
Issue:
The datasheet describes Pixel resolution and Display resolution. What is the difference?

Product Line:
Magelis HMI,iPC

Resolution:
Pixel resolution and display resolution are two different things. The Pixel Resolution defines how detailed an individual pixel will appear on the screen.

The Pixel Resolution of the HMIDM9521 is 1024x1024.  The images would appear blurry say at 10 x 10 compared to the 1024 x 1024 on the same display resolution.

See these image below as an example.

The display resolution is what we commonly all work with that defines the Height and Width of the screen.

Schneider Electric Sverige

Bilagor
Images.png [25.11 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj