{}

Våra varumärken

Impact-Company-Logo-English Black-01-177x54

Välkommen till Schneider Electrics webbplats

Välkommen till vår webbplats.
Hur kan vi hjälpa dig idag?
How can you set, change or remove the password on the Process drives using the Somove software?
Issue:
Customer wants to reset the password using Somove software.

Product Line:
Somove and Process Drive ATV630 and ATV930.

Environment:
All

Cause:
Reset the password using Somove.

Resolution:

On SoMove, going: Device -> Protection, you have the same features when using keypad`s: Main menu -> 4.Password .
Level1/Level2 corresponds to: PIN1/PIN2.

1. To set the password:





2. To change the password:





3. To remove password:



4. Protecting the SoMove file can be done by File/Project properties:







Schneider Electric Sverige

Utforska mer
Produkt:
Artiklar som kan vara till nytta
Utforska mer
Produkt: