How to know which GSD file to use for ATV71 with profibus card?
There have been 2 types of profibus card: VW3A3307 and VW3A3307S371
First card used was profibus DPV0 version (cyclic communication only) while second card was DPV1 (cyclic + possibility for acyclic communication)
See attached pdf for GSD file number.
Today the cards have the same reference VW3A3307 and on the label it is written DPV1.
If you see DPV0, use TELE0956.gsd. If you see DPV1, use TELE09CD.gsd.
GSD files are available on our web, under section ATV71 - software - profibus DPV0 files or profibus DPV1 files.
https://www.tscautomate.com/files/download/01HWUJN4RMMLPCGEBKMVFZYCISITIJTRND
https://www.tscautomate.com/files/download/01HWUJN4WUY43HV5YYDNF2NCYMV2GTITJJ

Schneider Electric Sverige

Bilagor
Difference DPV0 and DPV1.pdf [154.14 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj