PSO9.0 PowerLogic driver crashing the IO Server while communicating using MicrologicX(MTZ) protocol
Issue:
IO Server crashed in PSO9.0 while communicating using MicrologicX(MTZ) protocol
  • PSO 9.0 CU#2
  • PowerLogic Driver version is 4.3.6.1
Runtime Error!
R6025 – Pure virtual function call

Resolution:
Upgrade the PowerLogic driver to the latest version available on Exchange Community.
https://community.exchange.se.com/t5/EcoStruxure-Power-SCADA/PowerLogic-Driver-Pack-Latest-Release-for-PowerSCADA-7-40-or/m-p/150186

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj