SCADAPACK Battery Shelf life
On units that are under power most of the time, the batteries are expected to approach their shelf life, or approximately 7 – 10 years; depending on the environmental conditions to which they are exposed, and the total amount of power-off time during that period
As soon as battery level reached 3.1 v, It should give an alarm. And if battery level reached 3.0 v battery should be replaced.

Please find attached file for more information about "Battery Depletion" procedure.

If your batteries need to be replaced according to voltage threshold above, So please fill the form in the link attached below :
https://docs.google.com/forms/d/e/1FAIpQLSft15V7lpiQIgsKqff_8PsDho6Zo_WIEszViXizEmmHOtgsCQ/viewform

Schneider Electric Sverige

Bilagor
SCADAPack - Early RAM Battery Depletion.pdf [612.77 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj