Hot to Install a Driver in ClearSCADA?

To install a driver in ClearSCADA follow the following steps:
  1. Shut down the server.
  2. Use the ClearSCADA installation wizard.

  3. Click Next

  4. Click Modify

  5. Expand the server and select the driver you want to install press Next and follow the steps to finish the installation

    Any icon that displays a red cross indicates a component that will not be installed.

  6. Restart the Server after finishing the installation.
  7. Repeat the above steps on the other servers on your system. (On a Hot-Standby system, once you have installed the new driver(s) on a standby server, bring that server back online and synchronize it with the main server. Repeat the above steps with any other standby servers, then perform a manual changeover to upgrade one of the standby servers to main. Following this, install the driver(s) on the machine that was previously main, then bring that server back online.)

Schneider Electric Sverige

Utforska mer
Produktfamilj
Utforska mer
Produktfamilj