Sök bland vanliga frågor (FAQ)
What is the version compatibility for M340 NOE Module (Ethernet) and Processor
The following table shows compatible combinations for M340 NOE Module and M340 Processor:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008z1S3QAI&oid=00DA0000000abSm)
* In this case the NOE module will not be recognized as correct by the CPU when the application starts. An I/O error message will be displayed, as if a module other than an NOE were inserted in the slot.
* In this case the NOE module will not be recognized as correct by the CPU when the application starts. An I/O error message will be displayed, as if a module other than an NOE were inserted in the slot.
Publicerad för:Schneider Electric Sverige
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj