Why is the Input Current of Altivar 71 HD90N4 to HC50N4 range of drives less than the Output Current
The Input Current of Altivar 71 HD90N4 to HC50N4 range of drives is less than the output current because of the presence of the DC Choke (Lw).
The DC choke reduces the amplitude of the harmonics 5, 7, 11, 13......, thus causing the RMS current to reduce.

Schneider Electric Sverige

Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj