Which are the Encoder Option cards available for Altivar 71 along with their part numbers and specification
Six types of encoder cards are available depending on the Encoder Technology (Incremental or Absolute).

1.) RS 422 compatible differential outputs.
2.) Open collector outputs. (NPN)
3.) Push-pull outputs.
4.) Resolver.
5.) SinCos, SinCos Hiperface, EnDat or SSI.
6.) RS 422 compatible differential outputs with encoder emulation. (RS 422 ESIM)
These last three cards are available only with the following Altivar 71 Drives:

ATV71H***M3383
ATV71H***M3X383
ATV71H***N4383
Refer to attached file for part number and specification of encoder cards.

Schneider Electric Sverige

Bilagor
Encoder Option Cards.pdf [123.21 KB]
Utforska mer
Produktfamilj
Artiklar som kan vara till nytta
Utforska mer
Produktfamilj