Installing the 'SchneiderPLCUSBDriverSuite V14.15.0.0' returns the following error.:

Use the following steps to run the ps1 file named 'Release-PerUserDrivers.ps1' can be used to resolve the issue.
- Browse to the location you stored the ps1-file in File Explorer and choose; File-> Open Windows PowerShell.
- Type (part of) the name of the script.
- Press TAB to auto complete then name. Note: Do this even when you typed the name in full. ...
- Press ENTER to execute the script.
Note: This doesn’t uninstall the old driver versions, but it deletes any 'SchneiderPLCUSBDriverSuite' installer related
registry keys that causes Windows to detect and refuse the install/uninstall of the driver components..
registry keys that causes Windows to detect and refuse the install/uninstall of the driver components..
Publicerad för:Schneider Electric Sverige