How to get the firmware version of the BMENUA0100 module?
To get the firmware version of the BMENUA0100, its accessible from the webpage of the BMENUA0100 module:

firmware

If the module has his Rotary switch on “standard” security, the login is :
User : installer
Password : Inst@ller1

If the rotary switch has his Rotary switch on “secure, then fill it with the user and password that the customer has defined

Schneider Electric Sverige

Utforska mer
Produkt:
Artiklar som kan vara till nytta
Utforska mer
Produkt: