Is it possible to simulate IO Scanner Objects, such as the TM3BCEIP, in EcoStruxure Machine Expert - Basic simulator?

Issue:
Is it possible to simulate IO Scanner Objects, such as the TM3BCEIP, in EcoStruxure Machine Expert - Basic simulator?


Product Line:

EcoStruxure Machine Expert - Basic (V1.0, V1.1, V1.2)


Resolution:

No. IO Scanner objects, such as the TM3BCEIP, are not simulated while running the simulator of Machine Expert - Basic.

Schneider Electric Sverige

Utforska mer
Produkt:
Artiklar som kan vara till nytta
Utforska mer
Produkt: