Sök bland vanliga frågor (FAQ)
How to activate the automatic restart feature, in the ATS480 soft start.
Issue:
How to activate the automatic restart feature, in the ATS480 soft start.
Product Line:
ATS480
Environment:
Auto Restart
Cause:
n/a
Resolution:
Yes, from the Main menu, go to Menu 3 ( Complete Settings). Scroll down to menu 3.9 ( Error Warning Handling and press enter. Scroll down to Auto Fault Reset and press enter, set to yes and
press enter. Scroll down to Fault reset time and press enter and adjust , if needed and press enter again. Press the ESC key to get back to the Main Menu.
The following faults permit this function: PHF, FrF, CLF, USF.
The soft starter fault relay remains activated if this function is active. The run command must be maintained.
This function can only be used in 2-wire control.