Issue
From ETL v6.2 I am unable to extract the EPO/PSO custom tag historical trend data using ETL tool.
Environment
Power SCADA Operation (PSO) 2020 With ETL v6.2
EcoStruxure Power Operation (EPO) v2021 / v2022 With ETL v6.2
Cause
This is a known issue prior to ETL v6.2. However, from this version for custom tags we need additional configuration which is explained in Resolution section.
Resolution
When configuring ETL Job > PSO Extract task make sure to set Include Custom Topics In Mapping Operations = True
After this follow the normal process to configure remaining part of task. Above step will help ETL tool to load the custom tags while Loading Sources in “Mappings” tab of the tool.
But to extract historical trend data from EPO DB, then you may need to create the custom Topics.xml file as per below screen cap (also sample file attached with this article) and place it in ETL install folder [the default location ‘C:\Program Files\Schneider Electric\ETL (PowerSCADA)’] and configure all the custom tags as per below example.
Note:LegacyTopicID must be unique negative number.
Have a look in to attached example Topics.xml file for more info.
Publicerad för:Schneider Electric Sverige