How to configure the MBP_MSTR function block to have the status of the NOE Quantum module?
Context
To configure the MBP_MSTR function block in order to have the status of the NOE Quantum module, please proceed as in the example below:
The screenshot below shows the use of the MBP_MSTR function block in an FBD section. This Control Expert app has been lab tested and works well.
FBD_section
With MBP_MSTR, each network communication operations canning be triggered via the network has a function code which is assigned it. The availability of specific operations depends on both the type of network and the type of module you are using. The different function codes are listed in the table below.
Function_codes
Knowing that our client wishes to know the state of the link of the NOE Quantum, then the function code which interests him is the one allowing to obtain local statistics and according to the table below, it is 3. The structure of the MBP_MSTR control block varies according to the type of network you are using whether it be Modbus Plus, TCP/IP Ethernet, and SyMax Ethernet. Structure for TCP/IP Ethernet is described below.
Operational_FC
You will find in the screenshot below the values ​​of CONTROL in the application that I developed and tested in my lab for customer understanding.
Variable_editor
I specify that the NOE module is in slot 4 of the rack and that is why MBP_MSTR.CONTROL[5]=16#0004.
The Ethernet TCP/IP module's response to the local statistics commands of the MBP_MSTR block can be found in the databuf array (see information in the table below):
Eth_Network_Statistics
If we refer to the screenshot relating to the animation table of the application developed for the client, the NOE status is given with the MBP_MSTR_DATA[3].The detail of all the information contained in this word can be found in the online help of Control Expert.
Board_Status
Product Line
PLC Quantum, 140 NOE 311 00, 140 NOE 351 00, 140 NOE 771 00, 140 NOE 771 01, 140 NOE 771 10, 140 NOE 771 11

Environment
Microsoft Windows 10 64-bit (version 21H1 or newer), Microsoft Windows 10 64-bit Enterprise 2019 LTSC (version 1809), Microsoft Windows Server 2019 (standard 1809 version), Microsoft Windows 11 64-bit (version 21H1 or newer), Microsoft Windows Server 2022 (version 21H1 or newer), EcoStruxure Control Expert V15.3

Schneider Electric Sverige

Utforska mer
Produkt:
Utforska mer
Produkt: