Why can't I downgrade the BMXNGD0100?
This is due to a new NAND Flash hardware component introduced in Product Version (PV) 27 and greater.

If you have a BMXNGD0100 that is PV27 or greater, the lowest acceptable firmware level is v4.10.The downgrade procedure will fail if you attempt to downgrade the firmware below v4.10 with a PV27 or greater.

For more information on the BMXNGD0100, please visit SE.com.

Schneider Electric Sverige

Utforska mer
Produkt:
Artiklar som kan vara till nytta
Utforska mer
Produkt: