{}

Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
Prehľadávať FAQ
What is the difference between the XBTZ968 and the XBTZ9680 cables?

Issue

What is the difference between the XBTZ968 and the XBTZ9680 cables?

Product Line

Magelis XBT-G

Environment

XBTZ968

Resolution

Both cables have the same pinout and length. The difference between the two cables is the XBTZ9680 uses a right angle DB25 connector as opposed to a straight connector.

Schneider Electric Slovakia

Objavte viac
Rad:
Články, ktoré môžu byť užitočné
Objavte viac
Rad: