{}

Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
Prehľadávať FAQ
Is there system words available in the M340 to help me troubleshoot the READ_VAR and WRITE_VAR communication block?
There are a few system words to help.

%SW90 provides the maximum number of requests that the PLC can handle.
%SW86 indicates the number of messages being refused.  It should always be at 0.

Schneider Electric Slovakia

Objavte viac
Rad:
Články, ktoré môžu byť užitočné
Objavte viac
Rad: