Vitajte na webovej lokalite spoločnosti Schneider Electric
Vitajte na našej webstránke.
Prehľadávať FAQ
How can I reload the custom parameter set stored inside the drive memory from last saved on the ATV212 or S-Flex?
Issue: How can I reload the parameters stored in the drive from the factory or from last saved configuration on the ATV212 or S-Flex?
Product Line: ATV212 including the S-Flex enclosed drives.
Environment: All
Cause: Change in programming or application requires the drive to be reset to factory default settings and reload last saved custom parameter inside the drive memory
Resolution: If a program had been saved to the drive as using tyP set to 7, then the saved file can be restored by changing tyP to 8.