{}

Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
Prehľadávať FAQ
Sepam is showing a reverse rotation Alarm.
Issue
On the front display of the Sepam it is showing a reverse rotation Alarm.

Product Line
Sepam Series 40
Sepam Series 80

Cause
The Sepam is looking at the voltage phase rotation.  On the Sepam 40s it is looking for an ABC rotation.  The Sepam 80s it can be wired ABC or ACB.

Resolution
Sepam 40:
The only way to fix the reverse rotation alarm is to re-wire the voltages to an ABC rotation even if its a ACB rotation.  To help on the wiring please click here for the Sepam 40 wiring diagram.

Sepam 80:
One can just make the changes in SFT2841 by going to the General characteristics tab.  In the Electrical network box look for Phase rotation direction and select which rotation is needed.
Image 1

Schneider Electric Slovakia

Objavte viac
Rad:
Články, ktoré môžu byť užitočné
Objavte viac
Rad: