{}

Naše značky

Impact-Company-Logo-English Black-01-177x54

Vitajte na webovej lokalite spoločnosti Schneider Electric

Vitajte na našej webstránke.
Prehľadávať FAQ
When installing a NetShelter VED kit is it possible that the duct may cover more than one ceiling tile?
Issue:
Multiple ceiling tiles need to be cut.

Product Line:
NetShelter Vertical Exhaust Duct

Environment:
All versions and serial ranges.

Cause:

Where the VED Kit meets the ceiling, the VED covers more than one ceiling tile.

Resolution:
It's common that the duct will cover more than one ceiling tile. Consequently, more than one ceiling tile may need to be cut.

Schneider Electric Slovakia

Objavte viac
Rad:
Články, ktoré môžu byť užitočné
Objavte viac
Rad: