{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to connect the External Sensor CT for Micrologic 6 A/E/P/H (Residual Earth-Fault Protection)

Connection of current-transformer secondary circuit for external neutral Masterpact equipped with a Micrologic 6 A/E/P/H:
- shielded cable with 2 twisted pairs
- T1 twisted with T2
- maximum length 4 meters
- cable cross-sectional area 0.4 to 1.5 mm2
- recommended cable: Belden 9552 or equivalent.
For proper wiring of neutral CT, refer to instruction Bulletin 48041-082-03 shipped with it.
Do not remove Micrologic factory-installed jumper between T1 and T2 unless neutral CT is connected.

If supply is via the top, follow the shematics.
If supply is via the bottom, control wiring is identical; for the power wiring, H1 is connected to the source side, H2 to the load side.

Connection for signal VN is required only for power
measurements (3 Ø, 4 wires, 4CTs).

FA336173

Schneider Electric Thailand

Related products for Schneider Electric Thailand
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Related products for Schneider Electric Thailand
Range: