Search FAQs
Back UPS Pro - Unit sensitivity adjustment
Unit sensitivity
Adjust the sensitivity of the Back-UPS to control when it will switch to battery power; the higher the sensitivity, the more often the Back-UPS will switch to battery power.
1. Ensure the Back-UPS is connected to utility power, but is OFF.
2. Press and hold the POWER button for six seconds. The LOAD CAPACITY bar will flash on and off, indicating that the Back-UPS is in programming mode.
3. Press POWER again to rotate through the menu options. Stop at selected sensitivity. The Back-UPS will beep to confirm the selection.
![Back UPS Pro - Unit sensitivity adjustment Back UPS Pro - Unit sensitivity adjustment](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009M5OLQA0&oid=00DA0000000abSm)
Adjust the sensitivity of the Back-UPS to control when it will switch to battery power; the higher the sensitivity, the more often the Back-UPS will switch to battery power.
1. Ensure the Back-UPS is connected to utility power, but is OFF.
2. Press and hold the POWER button for six seconds. The LOAD CAPACITY bar will flash on and off, indicating that the Back-UPS is in programming mode.
3. Press POWER again to rotate through the menu options. Stop at selected sensitivity. The Back-UPS will beep to confirm the selection.
Released for:Schneider Electric Thailand
Related products for Schneider Electric Thailand
Range:
Related products for Schneider Electric Thailand
Range: