{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Cable size recommendation for surge protection SPD type 1 and type 2 according to IEC 60364

The conductor must resist a short-circuit current during the maximum protection system cutoff time.

IEC 60364 recommends at the installation incoming end a minimum cross-section of:
  • 4 mm² (Cu) for connection of Type 2 SPD
  • 16 mm² (Cu) for connection of Type 1 SPD (presence of lightning protection system).

Schneider Electric Thailand

Related products for Schneider Electric Thailand
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Related products for Schneider Electric Thailand
Range: