How can we help you today?
How to Calculation of Reactive Energy Based on the Application
Power Factor Correction for Transformer no-load compensation
The transformer works on the principle of Mutual Induction.
The transformer will consume reactive power for magnetizing purpose.
Following equivalent circuit of transformer provides the details of reactive power demand inside the transformer:
power factor correction
Power Factor Correction where Load and present
Power Factor is Known
The objective is to determine the requested reactive power Qc (kvar) to be installed, in order to improve the power factor cosφ and reduce the apparent power S.
For φ’ < φ, we’ll get: cosφ’ > cosφ and tanφ’ < tanφ
This is illustrated on the diagram in the left.
Qc can be determined from the formula : Qc = P. (tanφ - tanφ‘), which is deduced from the diagram.
Qc : power of the capacitor bank, in kvar
P : active power, in kW
tanφ: tangent of the phase angle - before compensation,
tanφ‘: tangent of the phase angle - after compensation
The parameters φ and tanφ can be obtained from the billing data, or from direct measurement in the installation.
The following table can be used for direct determination.
kvar table
Example:
Consider one 1000kW motor with cosφ 0.8 (tanφ = 0.75).
In order to get cosφ’= 0.95, it is necessary to install a capacitor
bank with a reactive power equal to
k x P, i.e. : Qc = 0.42 x 1000 = 420 kvar

Schneider Electric Thailand

Related products for Schneider Electric Thailand
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Related products for Schneider Electric Thailand
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.