Issue:
What is minimum firmware version required for the ATV71 or ATV61 to use the VW3A3316 Ethernet IP card?
Product Line:
VW3A3316
Cause:
ATV71 & ATV61 have minimum firmware required to use the VW3A3316 Ethernet IP card
Resolution:
This communication option card is fully supported with the version V1.5 IE 13 and above of the Altivar 61 firmware. This communication option card is only supported with the version V1.6 IE 19 and above of the Altivar 71 firmware. Specific versions of the Altivar 71 firmware are not supported.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand