What Protocols are Supported by the Panel Server ?Article available in these languages: Czech
Main protocols supported by the Panel Server range are listed in the table below.
Protocols | PAS400 (Entry) | PAS600 (Universal) | PAS800 (Advanced) |
---|
Modbus RTU | No | Yes | Yes |
Modbus TCP | Yes | Yes | Yes |
IEEE 802.15.4 Wireless | Yes | Yes | Yes |
Wi-Fi (2,4 and 5 GHz) | Yes | Yes | Yes |
Bluetooth | Yes | Yes | Yes |
HTTPS | Yes | Yes | Yes |
TLS 1.2 | Yes | Yes | Yes |
NTP / SNTP | Yes | Yes | Yes |
DHCP | Yes | Yes | Yes |
DPWS | Yes | Yes | Yes |
LoRa | No | No | No |
BacNET | No | No | No |
LPWAN | No | No | No |
Sigfox | No | No | No |
เผยแพร่สำหรับ:ชไนเดอร์ อิเล็คทริค Thailand