Pin | RS232 | RS485 |
1 | RxD | N.C. |
2 | TxD | N.C. |
3 | RTS | N.C. |
4 | N.C. | D1 / D+ |
5 | N.C. | D0 / D- |
6 | CTS | N.C. |
7 | N.C. | 5 Vdc |
8 | Common | Common |
CTS: Clear to Send
RTS: Ready To Send
RxD: Received Data
TxD: Transmitted Data
N.C.: No Connection
Yayımlanma amacı:Schneider Electric Turkey