搜尋常見問題
Can you mount 8910DPA contactors on DIN rail?
Issue:
8910DPA DIN mount options
Product Line:
Class 8910 Definite Purpose Contactors
Environment:
North American Products
Cause:
Mounting options
Resolution:
Yes, with the addition of the DIN rail mounting bracket, 9999DMB1. It is for use on 20-60A Type DPA contactors only.
8910DPA DIN mount options
Product Line:
Class 8910 Definite Purpose Contactors
Environment:
North American Products
Cause:
Mounting options
Resolution:
Yes, with the addition of the DIN rail mounting bracket, 9999DMB1. It is for use on 20-60A Type DPA contactors only.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: