{}
搜尋常見問題
Can the SR2A101FU be programmed from the front of the relay without using the PC and software?
Issue:
Programming a Zelio SR2 without a PC

Product line:
Zelio IEC Style Smart Relays

Environment:
Relays and Timers

Resolution:
Yes it can, but it has to be in LADDER language only.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: