搜尋常見問題
What are the contact ratings of the 9007MS/ML type limit switch?
Issue:
Needs to know the contact ratings of a 9007MS/ML limitswitch.
Product Line:
9007MS, 9007ML Limit Switch
Environment:
9007MS/ML
Resolution:
These limit switches have contact ratings of 300V AC and DC, at up to 10 amperes. Contact ratings may be higher than connector ratings
when using some of the prewired connector products.
Needs to know the contact ratings of a 9007MS/ML limitswitch.
Product Line:
9007MS, 9007ML Limit Switch
Environment:
9007MS/ML
Resolution:
These limit switches have contact ratings of 300V AC and DC, at up to 10 amperes. Contact ratings may be higher than connector ratings
when using some of the prewired connector products.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: