{}
搜尋常見問題
How do you order XVBC33, XVBC34 and XVBC38 to come with LED bulbs?
Bulbs, 10W maximum, are not included with these lens units. Order LED bulbs of proper color and voltage separately (see Digest 174, page 19-110, Table 19.337).

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: