搜尋常見問題
Can I use anything besides the APC provided mounting screws to rack mount my Rack PDU or ATS?
Issue
Can I use third party mounting hardware to mount my Rack PDU or Rack ATS in my Rack?
Product Line
Rack PDU Models
- AP95XX
- AP7XXX
- AP8XXX
Rack ATS Models
- AP77XX
- AP44XX
Environment
- All installation scenarios
Cause
Using any other screws can damage the internal wiring of the PDU or ATS and can be potentially dangerous to the end-user. This is noted in the user's manual of all Rack PDU or ATS as seen below.
Resolution
If you use screws other than those provided by APC to mount the Rack PDU or ATS, you will void your warranty. Use only the APC supplied mounting hardware on your device and/or adhere to any warnings on the product about screw lengths if the original hardware is unavailable.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: