{}

我們的品牌

Impact-Company-Logo-English Black-01-177x54

歡迎造訪施耐德電機全球網站

歡迎訪問我們的網站
搜尋常見問題
What control voltage is needed for an ATS01N1..FT softstart?
Issue:
Does the ATS01N1..FT need control voltage for running?


Product Line:
Altistart 01


Environment:
All


Cause:
N/A


Resolution:
The ATS01..FT models accommodate several control voltage options:
110 - 230Vac can be connected to terminal CL2 and neutral to CL1/0
24Vac or 24Vdc can be connected (+) to terminal 24V and (-) to CL1/0

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: