{}
搜尋常見問題
The NetShelter CX doors are not aligned. Can they be adjusted?
Issue:
NetShelter CX Door Misalignment

Product Line:
NetShelter CX

Environment:
All versions and serial ranges.

Cause:
The cause for an uneven door may not be known but it can be corrected.

Resolution:
Make sure the floor is even and, if not, adjust the leveling feet and level the cabinet.
Also, the doors may move slightly in transit. If this happens the hinges can easily be adjusted to fix this. Use a phillips head screwdriver to move the hinge as required.

施耐德電機Taiwan

探索更多
系列:
可能有幫助的文章
探索更多
系列: