Issue:
The soft start runs the motor in reverse when in generator mode.
Product Line:
ATS48, ATS22
Environment:
All Models and serial numbers
Cause:
Motor running in reverse
Resolution:
To change the direction of the motor swap two wires feeding the soft start at the generator.