搜尋常見問題
How can you break down the ETA status word 3201 on the ATV61 and ATV71 drives?
Issue:
Break down of ETA status word 3201 on the ATV61/ATV71 drives
Product Line:
Alitvar ATV61 and ATV71
Environment:
With Profibus option card
Cause:
Needs to know the bit breakdown for the ETA status word.
Resolution:
ETA status word for Word 3201
bit 0= Reserved
bit 1= Ready
bit 2= Running
bit 3= Fault
bit 4= Power section line supply present
bit 5= Reserved
bit 6= Reserved
bit 7= Alarm
bit 8= Reserved
bit 9= Command or Ref via network
bit 10= Referenced reached
bit 11= Reference outside of limit
bit 12= Reserved
bit 13= Reserved
bit 14= Stop via Keypad stop button
bit 15= Direction of motor 1=reverse 0=forward.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: