搜尋常見問題
What is the part number for the I/O extension option card for the ATV61/71 drives?
Issue:
Part number of I/O extension option card for the ATV61/71 drives?
Product Line:
Altivar Machines, Altivar 61, Altivar 71
Environment:
All
Cause:
Part number needed to order part
Resolution:
VW3A3201= Basic IO card gives you 4 more logic inputs, 2 logic outputs, 1 form C contact, Logic output and ptc input.
VW3A3202= Extended IO option card contains all of the basic IO options plus 2 more analog inputs, 2 analog outputs and 1 pulse input.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: