搜尋常見問題
How is Sepam 1000+ connected to existing core balance CTs?
The core balance CT interface ACE990 is used to match the measurement of an existing MV core balance CT with ratio 1/n (50=< n =< 1500) with that interface connected to the residual current input of Sepam 1000+.
Re-published to revised security level: 17 June 2008 by DRM
Applies To: Sepam 1000+ (Sepam Series 20 and Sepam Series 40)
Public
All content © 1992-2008 Schneider Electric
Legacy KB System (APS) Data: RESL166633 V2.0, Originally authored by LaVI on 06/20/2008, Last Edited by DaMi on 06/20/2008
Related ranges: Sepam series 40, ACE 9XX, Sepam series 20