搜尋常見問題
What is the maximum number of digital inputs the Sepam series 40 can have?
The Sepam 40 can have up to 10 digital inputs. Using the MES114 which has 10 digital input and 4 additional digital outputs. The Sepam series 40 comes with 4 digital output as standard.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: