搜尋常見問題
What are the dominate classes of Transfomer cooling?
There are four dominate classes of transformer cooling:
Class Definition
1. ONAN Oil Natural - Air Natural
2. ONAF Oil Natural - Air Force
3. OFAF Oil Force - Air Force
4. OFOD Oil Force - Oil Directed