搜尋常見問題
What causes the error: " Attempted IO operation (write) on READ-ONLY " when I go onto Vijeo Designer Webgate?
Issue:
The cause of the error: " Attempted IO operation (write) on READ-ONLY " when logged into Vijeo Designer Webgate
Product Line:
Vijeo Designer
Resolution:
You will get this error either due to the variables are not set for 'read/write' for data sharing. Or you are accessing Webgate without security.
If you do not enable Webgate security, you will only have read only access. Create a Security group and User and the error should go away.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: