搜尋常見問題
Can I use a HART enabled device with the M340 analog input module?
Yes, the BMXAMI0800 and BMXAMI0810 modules will support analog signals with HART protocol.
If HART information is part of the signal to be measured, a Telefast interface
ABE7CPA31E has to be used to filter this information which would disrupt the analog value.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: