搜尋常見問題
How do I resolve the error: "Application Has Halted Exception: Access Violation ComSystem.dlm:Koohi.cpp:line1078" in the Vijeo Designer simulator when using recipes?
Issue:
How do I resolve the error: Application Has Halted Exception: Access Violation ComSystem.dlm:Koohi.cpp:line1078"
Product Line:
Vijeo Designer
Resolution:
This error occur because the recipe variables are defined as internal variables. If you download to the target, it will
work fine. But if you need to run it in the simulator, you will need to change the Recipe variables to external and not internal type variables.
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: