搜尋常見問題
Is the backlight on a Magelis XBTGT replaceable?
The backlight on the Magelis XBTGT can be replaced on certain model.
Model | Catalog number |
XBTGT5230 | XBTZG43 |
XBTGT53*0 | XBTZG45 |
XBTGT53*0 PV03 or greater / XBTRGT54*0 | XBTZG45B |
XBTGT63*0 | XBTZG46 |
XBTGT7340 | XBTZG47 |
發佈於:施耐德電機Taiwan
探索更多
系列:
探索更多
系列: