搜尋常見問題
Lexium32 encoder connector plugs (type/specification and tools) used on the amplifier end of the encoder cable ?
Goals and Symptoms
Lexium32 encoder connector plugs (type/specification and tools)
used on the amplifier end of the encoder cable ?
Causes and Fixes
We use with our encoder cables:
Y-ConPlug-31 (Plug) and Y-ConIP20Lock-10
(IP20-Strain relief with vibration resistant locking clips),
The tools reqired for cable assembly can be ordererd directly
from the manufacturer:
Crimping tool for encoder connector RJ45 10 pins:
Yamaichi Y-Con Tool-11, Y-Con Tool-20, Y-Con Tool-30
( www.yamaichi.com )
Crimping tool for encoder connector M23:
Coninvers SF-Z0007 ( www.coninvers.com )
Crimping tool for power connector M23/M40:
Coninvers SF-Z0008 ( www.coninvers.com )
Please look to the attached catalogues for connector and tools
Attachments
(Removed File URL: 201460_E336/RJ45.zip)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/f86ffec6312f0352c12576d6004219c3/fl_block_5/0.60E?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL201460 V1.0, Originally authored by BeBr on 02/26/2010, Last Edited by BeBr on 02/26/2010
Related ranges: Lexium 32